AXIS#.UNIT.ACCROTARY
Description
AXIS#.UNIT.ACCROTARY sets the acceleration/deceleration units when the motor type (AXIS#.MOTOR.TYPE ) is rotary.
Type | Description |
---|---|
0 |
|
1 |
RPS/s |
2 |
deg/s2 |
3 |
Custom Units/s2 |
4 | rad/s2 |
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 4 |
Default Value |
0 |
Data Type |
Integer |
See Also |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.UNIT.ACCROTARY | 0x5010 | 0x3 | USINT | - | - | RW | False |
AXIS2.UNIT.ACCROTARY | 0x5110 | 0x3 | USINT | - | - | RW | False |