AXIS#.ZEROT
Description
AXIS#.ZEROT is the time value for the motor velocity to be within AXIS#.ZEROV before the drive considers the motor to be at zero velocity.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
|
Renamed from AXIS#.DISTVTHRESH | 02-03-00-000 |
General Information
Type |
Read/Write |
Units |
ms |
Range |
1 to 30,000 ms |
Default Value |
6 ms |
Data Type |
Integer |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.ZEROT |
0x5002 |
0x3 | UDINT | - | - | RW | False |
AXIS2.ZEROT | 0x5102 | 0x3 | UDINT | - | - | RW | False |