AXIS#.OPMODE
Description
AXIS#.OPMODE specifies the operation mode of the axis. You must also use AXIS#.CMDSOURCE to set the source of the command to the axis.
The operation mode values can be set as follows:
Mode |
Description |
---|---|
0 |
Current (torque |
1 |
Velocity operation mode |
2 |
Position operation mode |
AXIS#.OPMODE can be changed while the axis is enabled or disabled. If you are using the terminal to change the operation mode, it is recommended that you disable the axis before changing the operation mode. If you change the operation mode from the terminal while the axis is enabled, the system may experience a step change in demand.
Example
Set the source of the command to a TCP/IP channel and the desired operation mode to velocity:
-->AXIS1.CMDSOURCE 0
-->AXIS1.OPMODE 1
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 2 |
Default Value |
0 |
Data Type |
Integer |
Stored in Non Volatile Memory |
Yes |
Gantry Mode
If the axis is in Gantry Mode (CMDSOURCE = 4), then this opmode setting has no effect until the CMDSOURCE is set to something other than 4 – Gantry.
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.OPMODE | 0x5000 | 0x5 | USINT | - | - | RW | False |
AXIS2.OPMODE | 0x5100 | 0x5 | USINT | - | - | RW | False |