FB#.RESKTR
Description
This parameter sets the resolver nominal transformation ratio. It affects the resolver excitation output amplitude.
The value can be obtained from the resolver data sheet.
Context
See Feedback Devices.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0.001 to 50.000 |
Default Value |
0.5 |
Data Type |
Float |
See Also |
N/A |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
FB1.RESKTR | 0x3500 | 0x4 | UDINT | - | - | RW | False |
FB2.RESKTR | 0x3501 | 0x4 | UDINT | - | - | RW | False | |
FB3.RESKTR | 0x3502 | 0x4 | UDINT | - | - | RW | False | |
FB4.RESKTR | 0x3503 | 0x4 | UDINT | - | - | RW | False | |
FB5.RESKTR | 0x3504 | 0x4 | UDINT | - | - | RW | False |