AIN.CUTOFF
Description
AIN.CUTOFF sets the break frequency in Hz for two cascaded single-pole low-pass filters on the hardware command input. Since the two poles are cascaded at the same frequency, the -3 dB frequency is 0.64*AIN.CUTOFF in hertz and the 10% to 90% step response rise time is 0.53/AIN.CUTOFF in seconds.
Suggested operating values are as follows:
- Analog torque
Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist opmode: 5 kHz
- Analog velocity opmode: 2.5 kHz
- General purpose analog input high resolution: 500 Hz
General Information
Type |
NV Parameter |
Units |
Hz |
Range |
0 to 10,000 Hz |
Default Value |
5,000 Hz |
Data Type |
Float |
Start Version |
M_01-00-00-000 |
Variants Supported
*In SynqNetSynqNet is a digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Index/Subindex |
Object Start Version |
|
---|---|---|
5000h/0 |
M_01-00-00-000 |
Related Topics