AIN.UVFTHRESH

Description

This parameter defines the under voltage threshold for analog input. If AIN.VALUE is less than AIN.UVFTHRESH, and AIN.MODE = 3 (user defined fault mode), an under voltage fault is generated.

General Information

Type

NV Parameter

Units

V

Range

-10 to 10

Default Value

-10V

Data Type

Float

Start Version

M_01-13-09-000

Variants Supported

*In SynqNetClosedSynqNet is a digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Related Topics

Analog Input | AIN.MODE | AIN.UVWTHRESH | AIN.OVFTHRESH | AIN.OVWTHRESH