AOUT.MODE
Description
AOUT.MODE sets the analog output functionality.
AOUT.MODE |
Description |
---|---|
0 |
User variable. The analog output signal is determined by the user (using AOUT.VALUEU). |
1 |
Actual velocity. The analog signal describes the current velocity value (VL.FB). |
2 |
Velocity error. The analog signal describes the velocity error value. |
3 |
Velocity command. The analog signal describes the velocity command value. |
4 |
Actual current. The analog signal describes the actual current value. |
5 |
Current command. The analog signal describes the current command value. |
6 |
Actual position. The analog signal describes the current position value. |
7 |
Position error. The analog signal describes the position error value. |
8 |
Triangle wave. The analog signal is a triangle wave (sawtooth pattern). |
9 |
Debug mode. In this mode the user can define a drive variable to monitor via the analog output (AOUT.VALUEU). |
10 |
Unfiltered Velocity (VL.FBUNFILTERED) |
11 |
Filtered Velocity - 10Hz Lowpass (VL.FBFILTER) |
12 | SynqNet![]() |
Example
You can use AOUT.MODE and AOUT.VALUEU to configure an output signal as follows:
-->AOUT.MODE 0
-->AOUT.VALUEU 5
-->AOUT.VALUEU 4.33
General Information
Type |
NV Parameter |
Units |
N/A |
Range |
0 to 12
|
Default Value |
0 |
Data Type |
Integer |
Start Version |
M_01-00-00-000 |
Index/Subindex |
Object Start Version |
|
---|---|---|
3470h/1 |
M_01-00-00-000 |
Related Topics