COGCOMP.EN
Description
If the COGCOMP.EN is set to one, the current regulator will add a feedforward current depending on the actual feedback position (PL.FB ) stored in the cogging compensation correction value (COGCOMP.CORRECTIONTABLE).
General Information
This content is not applicable to KAS.
Type |
NV Parameter |
Units |
N/A |
Range |
0 to 1 |
Default Value |
0 |
Data Type |
Integer |
Start Version |
M_01-14-06-001 |
Fieldbus![]() |
Index/Subindex | Object Start Version |
---|---|---|
540Fh/0 |
M_01-14-06-001 |