DRV.DISSOURCESMASK
Description
DRV.DISSOURCESMASK is a bitwise parameter that returns all possible causes of a drive disable. If a bit is set, the drive can be disabled for this reason.
The return value specific bits are as follows:
Bit | Status and Response |
---|---|
0 | Software triggered disable |
1 | Fault exists |
2 | Hardware Enable input inactive |
3 | In-rush relay state prevents enable |
4 | Initialization not complete |
5 | Controlled stop requested from digital input |
6 | Field bus requested disable |
7 | AKD-C requested disable (AKD-N only) |
8 | Pre-charge successful (AKD-C only) |
10 | AKD-C download mode disabled all AKD-Ns |
For most AKD models, this parameter will return the value 63.SynqNet is a digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices version of the drive, the parameter will return the value 127.
For AKD-N, this parameter will return the value 179. For AKD-C, this parameter will return the value 286.
General Information
Type |
R/O parameter |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
Integer |
Start Version |
M_01-07-00-000 |
Related Topics