FBUS.SYNCWND
Description
This parameter sets symmetrically arranged window around the desired sync distance.
General Information
Type |
NV Parameter |
Units |
ns |
Range |
0 to 1,000,000 ns |
Default Value |
50,000 ns |
Data Type |
Integer, U2 |
See Also |
Appendix B: Fieldbus |
Start Version |
M_01-00-00-000 |
Fieldbus |
Index/Subindex |
Object Start Version |
---|---|---|
3496h/3 |
M_01-00-00-000 |