GUI.DISPLAY
Description
This parameter reports to the GUI"Graphical User Interface"
A GUI is a type of user interface which allows people to interact with a computer and computer-controlled devices what the drive currently is displaying. For all GUI commands, the data is compressed and formatted for the GUI, not for the user.
General Information
Type |
R/O Parameter |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
Display |
See Also |
N/A |
Start Version |
M_01-00-00-000 |