IL.IVFB
Description
IL"Instruction list"
This is a low-level language and resembles assembly.IVFB is an offset value that is added to the measured current in the u-winding of the motor. This value is used for compensating for an error in the current measurement. The drive measures 256 times the current in the u-winding when powering-up the drive. Afterward, the drive calculates the average value of the measured current and uses this value for the offset value.
General Information
Type |
R/O Parameter |
Units |
A |
Range |
± Drive peak current (DRV.IPEAK) |
Default Value |
0 A |
Data Type |
Float |
See Also |
N/A |
Start Version |
M_01-00-00-000 |
Related Topics