IL.KPLOOKUPVALUES
Description
Retrieves the Current Loop Gain Scheduling Table in a comma delimited table.
This table is 256 records long, and the table will return values in the following format:
-->IL"Instruction list"
This is a low-level language and resembles assembly.KPLOOKUPVALUES
Index Value
0, 100.000
1, 100.000
2, 100.000
3, 100.000
4, 100.000
5, 100.000
6, 100.000
7, 100.000
8, 100.000
9, 100.000
10, 100.000
General Information
Type |
R/W Parameter |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
Table |
See Also |
|
Start Version |
M_01-04-00-000 |
Related Topics