MOTOR.RTYPE
Description
This parameter defines the type of thermal resistor used inside of the motor to measure motor temperature. The following resistor types are supported:
For firmware versions prior to 01-10-02-000, parameter range is 0 to 1.
| MOTOR.RTYPE | Thermal Resistor Type |
|---|---|
| 0 | PTC |
| 1 | NTC |
For firmware versions 01-10-02-000 and later, parameter range is 0 to 255.
| MOTOR.RTYPE | Thermal Resistor Type |
|---|---|
| 0 | Single PTC |
| 1 | Single NTC |
| 2 | KTY83-110 |
| 3 | KTY84-130 |
| 4 | PTC + KTY83-110 |
| 5 | Thermal switch |
| 255 | No sensor |
-
-
For firmware versions 01-09-00-000 and later, this parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET = 1.
General Information
|
Type |
NV Parameter |
|
Units |
N/A |
|
Range |
0 to 1 For firmware version 01-10-02-000 and later, range is 0 to 255. |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
50FEh/0 |
M_01-00-00-000 |
Related Topics