MOTOR.TEMPWARN

Description

This parameter is used to configure the motor temperature warning level as a resistance threshold of the motor PTC.

A zero value prevents any warning from being created.

General Information

Type

NV Parameter

Units

Ω

Range

0 to 2,000,000,000 Ω

Default Value

0 Ω = switched off

Data Type

Integer

See Also

MOTOR.TEMP

Start Version

M_01-00-00-000

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3453h/0

M_01-00-00-000

Related Topics

Motor View