VL.ARZQ1 TO VL.ARZQ4
Description
VL.ARZQ1 sets the Q (quality factor) of the zero (numerator) of AR filter 1. This value is QZ in the approximate transfer function of the filter:
AR1(s) = [s²/(2πFZ)²+s/(QZ2πFZ) + 1]/ [s²/(2πFP)² +s/(QP2πFP) + 1]
The following block diagram describes the AR filter function; note that AR1 and AR2 are in the forward path, while AR3 and AR4 are applied to feedback:
AR1, AR2, AR3 and AR4 are used in velocity and position mode, but are disabled in torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist mode.
Discrete time transfer function (applies to all AR filters)
The velocity loop compensation is actually implemented as a digital discrete time system function on the DSP. The continuous time transfer function is converted to the discrete time domain by a backward Euler mapping:
s ≈ (1-z-1)/t, where t = 62.5 µs.
The poles are prewarped to FP and the zeros are prewarped to FZ.
General Information
Type |
R/W Parameter |
Units |
N/A |
Range |
0.1 to 5 |
Default Value |
VL.ARZQ1: 0.707 VLARZQ2 to VLARZQ4: 0.5 |
Data Type |
Float |
See Also |
VL.ARPF1 TO VL.ARPF4 , VL.ARPQ1 TO VL.ARPQ4 , VL.ARZF1 TO VL.ARZF4 |
Start Version |
M_01-02-00-000 |
Fieldbus![]() |
Index/Subindex | Object Start Version | |
---|---|---|---|
3406h/D |
M_01-02-00-000 | ||
3406h/E |
|||
3406h/F |
|||
3406h/10 |
Related Topics