VL.OBSBW
Description
This parameter sets the bandwidthIn computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz of the observer in Hz. The observer passes the velocity feedback through a PID
"Proportional-Integral-Derivative"
A PID controller is a generic control-loop feedback mechanism widely used in industrial control systems.
An "error" occurs when an event or a disturbance triggers off a change in the process variable.
A PID controller attempts to correct the error between a measured process variable and a desired setpoint by calculating and then outputting a corrective action that can adjust the process accordingly control loop that behaves like a low-pass filter with a bandwidth of VL.OBSBW.
General Information
Type |
NV Parameter |
Units |
Hz |
Range |
10 to 4,000 Hz |
Default Value |
30 Hz |
Data Type |
Float |
See Also |
N/A |
Start Version |
M_01-03-00-004 |
Index/Subindex |
Object Start Version |
|
---|---|---|
51BAh/0 |
M_01-03-00-004 |
Related Topics