INSERT![This function or function block supports PLCopen motion PLCopen motion icon](../Resources/Images/Icon_PLCopen.png)
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Insert characters in a string.
Inputs
IN : STRING Character string
STR : STRING String containing characters to be inserted
POS : DINT Position of the first inserted character (first character
position is 1)
Outputs
Q : STRING Modified string.
Remarks
The first valid character position is 1. In FFLD language, the operation is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung.
In IL"Instruction list"
This is a low-level language and resembles assembly, the first input (the string) must be loaded in the
current result before calling the function. Other arguments are operands of the function,
separated by comas.
ST Language
Q := INSERT (IN, STR, POS);
FBD Language
FFLD Language
(* The function is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)
IL Language:
See also