FunctionMLAxisReadVelPipe Network motion icon

Description

Return the actual velocity of the axis, based on the data provided by the drive's feedback deviceClosedA process whereby some proportion of the output signal of a system is passed (fed back) to the input. In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position.

AKD, S300, S700 drives: The actual velocity is calculated internally by the drive. The 'Velocity Actual Value' object (CoE object 0x606C, subindex 0) must be included in the drive's Input (Tx) PDOClosedPDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. data for the controller to read the axis actual velocity from the drives. This can be added via the PDO Editor Tab. The 'Velocity Actual Value' object is included by default in the AKD PDOs 0x1B20, 0x1B22, and 0x1B23.

Arguments

Input

ID

Description

Pipe network identifier of the axis block.

 

Data type

DINT

 

Range

—

 

Unit

N/A

 

Default

—

Output

Velocity

Description

The actual velocity of the axis.

 

Data type

LREAL

 

Unit

User unit/sec

Related Functions

MLAxisReadActPos

MLAxisReadTq

Example

Structured Text

 

Axis1_Velocity := MLAxisReadVel(PipeNetwork.Axis1 ) ;

 

Ladder Diagram

MLAxisReadVel: LD example

Function Block Diagram

MLAxisReadVel: FBD example

Go back to the top of the page [Top]