Function BlockDriveParamStrReadPLCopen motion iconPipe Network motion icon

Description

This function block reads a single drive parameter by sending an ASCII command to a drive. The value returned is the string response from the drive.


  • This differs from DriveParamRead in that the drive response is not parsed. DriveParamRead parses the drive response and returns the numeric value of the parameter and the units found that represent that parameter. Since DriveParamStrRead returns the drive response directly, it can be used to read parameters that have string representations, such as the AKD2G’s AXIS#.FAULTMSG# parameters.

Figure 7-188: DriveParamStrRead

Arguments

Input

Execute

Description

Executes the Function BlockClosedA function block groups an algorithm and a set of private data. It has inputs and outputs.

Data type

BOOL

Range

0, 1

Unit

N/A

Default

—

Drive

Description

The address of the drive from which data is read.

Data type

INT

Range

—

Unit

N/A

Default

—

Param

Description

The parameter to read.

Data type

STRING

Range

—

Unit

N/A

Default

—

Output

Done

Description

Indicates whether this function block has completed without error.

Data type

BOOL

Unit

N/A

Error

Description

Indicates whether this function block call has completed with error:

Data type

BOOL

Unit

N/A

ErrorID

Description

The DriveParamStrRead error result if Error is TRUE (see list of Error Codes in table below). Upon success, Error is set to zero.

Data type

DINT

Unit

N/A

Value

Description

The value of the drive parameter. Value is only set when the function block has successfully completed.

Data type

STRING

Unit

N/A

Usage

Use this FB to read drive parameters that are not supported by other function blocks. Examples would be motor temperature, drive bus voltage, Present drive limit settings, present regen loading, drive display, and fault history.

Related Functions

DriveParamRead, DriveParamWrite

Example

Structured Text

            (* Read AXIS1.FAULTMSG1 on first AKD2G Drive on EtherCAT network *)

(* The code continually calls the FB (without re-executing it) until the first execution is done, then reads the returned value from the drive and reset the FB *)
IF ReadFaultMsg Then
  Inst_DriveParamStrRead1(True, 1001, 'AXIS1.FAULTMSG1' );
End_If;

On Inst_DriveParamStrRead1 Do
   FaultMsg := Inst_DriveParamStrRead1.Value; (* Reads the returned value from the drive *)
  Inst_DriveParamStrRead1(False, 1001, 'AXIS1.FAULTMSG1');
ReadFaultMsg := False; (* Reset the FB *)
End_DO;