MC_InitAxisFeedback
Description
This function block initializes a PLCopen
A vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML Digitizing Axis position data. A call to this function is automatically generated when the application is compiled, based on the data entered in the PLCopen Axis Data dialog.
Figure 7-124: MC_InitAxisFeedback
Arguments
For more detail on how inputs and outputs work, refer to PLCopen Function Blocks - General Rules
Input
|
En |
Description |
Request to Initialize a PLCopen Digitizing Axis |
|
Data type |
BOOL | |
|
Range |
0,1 | |
|
Unit |
N/A | |
|
Default |
- | |
|
AxisNumber |
Description |
Digitizing Axis Number |
|
Data type |
UINT | |
|
Range |
[1,256] | |
|
Unit |
none | |
|
Default |
- | |
|
FeedbackPDOIndex |
Description |
The object Index through which the feedback data is sent. |
|
Data type |
UINT | |
|
Range |
[0,65536] | |
|
Unit |
N/A | |
|
Default |
- | |
|
FeedbackPDOSubIndex |
Description |
The sub index of the object through which the feedback data is sent to controller. |
|
Data type |
UINT | |
|
Range |
[0,255] | |
|
Unit |
||
|
Default |
||
|
FeedbackDataResolution |
Description |
The resolution of the Encoder |
|
Data type |
UINT | |
|
Range |
[1,32] | |
|
Unit |
N/A | |
|
Default |
- |
Output
|
OK |
Description |
Indicates the initialization is complete See more details here. |
|
Data type |
BOOL |
|
| ErrorID |
Description |
Indicates if the call failed or succeeded. If the call succeeds, will be set to 0. |
|
Data type |
DINT |
Example
Structured Text
(* MC_InitAxisFeedback ST"Structured text" A high-level language that is block structured and syntactically resembles Pascal example *)
// Initialize the digitizing Axis (Axis #3) with the Feedback object 0x60E4 subIndex 2.
Encoder resolution is 25bits.
MC_InitAxisFeedback(3, 16#60E4, 16#02, 25);
[Top]