FunctionMLFB_JogPipe Network motion icon

Description

This function is defined to jog an axis in the selected direction at a defined speed. The En input (FFLD editor only) must be high. Typically wired to the rail. The AxisID selects the axis to jog. The JogPlus and JogMinus inputs select the direction the motion will occur in. Only one of these inputs should be enabled at a given time. If both are selected the motion will stop. If other motion is active when the jog is requested that motion will be aborted and the jog will start.

The following figure shows the function I/O

Figure 7-241: Kollmorgen UDFB Jog for PipeNetwork

Arguments

Input

En Description Enables execution (FFLD only )
 

Data type

BOOL
  Range —
  Unit N/A
  Default —
AxisID Description ID Name of the Axis
 

Data type

DINT
  Range —
  Unit N/A
  Default —
JogPlus Description Enables a Jog in the plus direction
 

Data type

BOOL
  Range [0 , 1]
  Unit N/A
  Default —
JogMinus Description Enables a Jog in the Minus direction
 

Data type

BOOL
  Range [0 , 1]
  Unit N/A
  Default —
Speed Description Rate at which the axis will move
 

Data type

LREAL
  Range —
  Unit User unit/sec
  Default —

Output

InMotion Description Jogging is active when TRUE
 

Data type

BOOL
  Range N/A

Usage

This function is used to command motion in a designated direction at a defined rate. This may be used where continuous motion required as in a conveyor system, or in a setup mode for manually jogging the axis. Motion will start when the JogPlus or JogMinus input is true. It will stop when the input goes false. This function is used with the Pipe Network motion engine.

Related Functions

MLAxisMoveVel

Example

Structured Text

//Jog Axis1 at 6000 user units a second when JogPlus or JogMinus variables are TRUE

//Stop motion on falling edge of either variable

MLFB_Jog( PipeNetwork.AXIS1, JogPlus, JogMinus, 6000 );

Ladder Diagram

Function Block Diagram

Go back to the top of the page [Top]