FunctionMLSyncInitPipe Network motion icon

Description

Initializes a synchronizer Pipe Block. Returns TRUE if the function succeeded.

This FB is automatically created in the compiled code of a Pipe Network.

This function block is part of the MLPN_CREATE_OBJECT to initialize the Pipe Network. It is called at the beginning of an application program with the function call:

PipeNetwork(MLPN_CREATE_OBJECTS);

Arguments

Input

BLockID

Description

Name of the Pipe Network Block

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

n/a

 

Default

—

ModuloPosition

Description

The modulo distance

 

Data type

LREAL

 

Range

—

 

Unit

User unit

 

Default

—

CurveType

Description

The curve type to the motion when starting and stopping synchronization. Option are Parabolic or Polynomial

 

Data type

DINT

 

Range

[1 , 2] (1 = Parabolic, 2 = Polynomial)

 

Unit

n/a

 

Default

—

DeltaS

Description

The Distance to get in or out of synchronization. This parameter is used in the  MLSyncStart and MLSyncStop FunctionBlocks

 

Data type

LREAL

 

Range

—

 

Unit

User unit

 

Default

—

Output

Default (.Q)

Description

Function BlockClosedA function block groups an algorithm and a set of private data. It has inputs and outputs. Execute Successfully

See more details here.

 

Data type

BOOL

 

Unit

n/a

Related Functions

MLSyncWriteDeltaS

Example

Structured Text

//Initialize  a synchronizer  Pipe Block named “ SYN” with a modulo of 360, Curve Type of Parabolic, and a distance (DeltaS) of 30 to get in and out of synchronization
MLSyncInit( PipeNetwork.SYN, 360, 1, 30 );

Ladder Diagram

MLSyncInit: LD example

Function Block Diagram

MLSyncInit: FBD example