FunctionMLTrigInitPipe Network motion icon

Description

Initializes a Trigger object for use in a PLCClosed"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events Program. FunctionClosedA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. block is automatically called if a Trigger Block is added to the Pipe Network, with user-defined settings entered in the Pipe Blocks Properties screen.

The Trigger object monitors a selected Fast InputClosedThe inputs are taken into account at each cycle depending on the system periodicity (for example each millisecond). Under certain circumstances this can be insufficient when more accuracy is needed, or if a quick response is required from the system. To fill the gap, a drive may have some Fast Input connections (generally one or two). When an event happens that triggers a Fast Input (e.g. when a sensor sends a rising edge), the detection of a signal occurs faster (which can be 1000 times more accurate than the system periodicity). Then the timestamp associated with this input can be provided to the IPC to take corrective action and captures the time of a rising or falling edge event. With the time and pipe position information the Trigger object extrapolates the axis position when the Fast Input event occurred.

Parameters to enter include the name of the Pipe Block, the Axis where the Fast Input is located, the number of the desired Fast Input, and whether to trigger on the rising or falling edge of the input.


  • Trigger objects are normally created in the Pipe Network using the graphical engine. Then you do not have to add MLTrigInit function blocks to their programs. Parameters are entered directly in pop-up windows, and the code is then automatically added to the current project.

Arguments

Input

BlockID

Description

ID number of a created Pipe Block

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

N/A

 

Default

—

     

Input_Axis

Description

Name of the axis where the Fast Input is located

 

Data type

STRING

 

Range

—

 

Unit

N/A

 

Default

—

     

InputID

Description

ID number of the Fast Input

0 = Touch Probe 1 / Capture Engine 0

1 = Touch Probe 2 / Capture Engine 1

Range is [0,1]

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

N/A

 

Default

—

     

EdgeID

Description

Trigger at rising or falling edge of Fast Input. Enter 1 for rising edgeClosedA rising edge is the transition of a digital signal from low to high. It is also called positive edge, 2 for falling edge, and 0 disables the Fast Input

 

Data type

DINT

 

Range

[0 , 2]

 

Unit

N/A

 

Default

1 (Rising edge)

Output

Default (.Q)

Description

Returns TRUE if function block is executed

See more details here.

 

Data type

BOOL

 

Unit

N/A

Return Type

BOOL

Related Functions

MLTrigIsTrigged

MLTrigReadPos

MLTrigClearFlag

MLAxisRstFastIn

See Also

Example

Structured Text

//Create and Initiate a Trigger Pipe Block named “Trigger” and set it up to receive the trigger signal from Axis1, capture engine 0, and the rising edge of the signal
TRIGGER := MLBlkCreate( 'TRIGGER', 'TRIGGER' );
MLTrigInit( TRIGGER, 'Axis1', 0, 1 );

Ladder Diagram

MLTrigInit: LD example

 

Function Block Diagram

MLTrigInit: FBD example