ACTION#.TASKID
Description
Some tasks require a task ID to specify what is acted upon. For example, if setting the value of DOUT2 from the source, then ACTION#.TASK = 1 (set Digital Output from Source), and ACTION#.TASKID = 2.
ACTION#.TASK must be set before ACTION#.TASKID. If ACTION#.TASK is modified, then the range and units of ACTION#.TASKID may be modified, and the value will be defaulted.
Not all tasks require a task ID.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
Depends on ACTION#.TASK |
|
Default Value |
Depends on ACTION#.TASK |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported