ACTION#.TASKTEXT
Description
This parameter defines the text associated with an ACTION Task.
To clear the text stored, use issue: ACTION#.TASKTEXT clear to remove the text and commands.
Actions Using TASKTEXT:
- 26: Command Buffer – see Command Buffer for more details.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-02-04-000 |
|
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
|
|
Data Type |
String |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.