FB#.STOREMULTITURN.BITS
Description
The number of most significant single-turn bits (power of 2 counts) used to determine if the position stored is valid after power cycle and ensures the motor did not move while the power was off. See Example Configuring FB#.STORE.MULTITURN.BITS.
| Bits | |
|---|---|
| 2 (default)-8 | The number of single turn most significant bits. |