PROFINET.USEMODULECFG
Description
This command controls where the drive obtains the telegram configuration. When set to 1 (default), the drive uses the telegram setting from the module configuration in the PROFINET master. When set to 0, the drive uses the telegram setting specified in AXIS#.PROFINET.TELEGRAMID (P922).
| Value | Description |
|---|---|
| 0 |
Drive uses the telegram specified from AXIS#.PROFINET.TELEGRAMID (P922) |
|
1 (default) |
Drive uses telegram configuration from the sub-module configuration in the PROFINET master. |
-
- When this keyword is set to 1 (use PLC
"Programmable Logic Controller"
A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines.
Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events configuration), AXIS#.PROFINET.TELEGRAMID and AXIS#.PROFINET.SUPPTELEGRAMID keywords are set to read only.
For more information, see .
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-04-05-000 |
General Information
| Type | Read/Write |
| Units |
N/A |
| Range | 0 to 1 |
| Default Value | 1 (Use sub-module configuration from PLC) |
| Data Type | Integer |
| Stored in Non Volatile Memory | Yes |
Variants Supported
PROFINET drives: AKD2G-SPP