REC.DONE
Description
REC.DONE indicates that the recorder has finished recording. This value is reset to 0 when the recorder trigger is set. The drive also resets this value when the recording has finished or when REC.OFF is executed.
Examples
Code
Indicates that recording has not completed, either because the triggering has not been completed or that the data capturing is ongoing.
-->REC.DONE 0
Context
For more information see Scope.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
See Also |
REC.ACTIVE, REC.OFF |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.