REC.NUMPOINTS
Description
REC.NUMPOINTS specifies the number of points (samples) to record.
Examples
Code
To record the maximum 10,000 samples:
-->REC.NUMPOINTS 10000
Context
For more information see Scope.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
1 to 10,000 |
|
Default Value |
1,000 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.