REC.TRIGPARAM
Description
REC.TRIGPARAM sets the parameter the recorder uses to trigger the capture.
This parameter is not used when REC.TRIGTYPE is 0 (Immediate) or 1 (On Next Command).
The parameters that can be used with REC.TRIGPARAM are listed by REC.TRIGPRMLIST. The parameters that can be used as a trigger also have the [Trigger] tag in their DRV.HELP output.
Examples
Context
For more information see Scope.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
AXIS1.IL |
|
Data Type |
String |
|
See Also |
|
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.