VBUS.INRUSHON
Description
This parameter returns the voltage at which the DC bus inrush relay closes.
Examples
Usage
The drive configures this parameter based on power electronics component ratings. When the measured DC bus voltage VBUS.VALUE is greater than VBUS.INRUSHON, the drive closes the inrush relay.
Context
For more information on DC bus operation, refer to Power.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-02-03-000 |
General Information
|
Type |
Read Only |
|
Units |
Vdc |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer |
| See Also | VBUS.VALUE, VBUS.INRUSHOFF |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants supported.