AIN.OFFSET
Description
AIN.OFFSET sets the analog offset, which is added to the analog input command to the drive. This value compensates for the analog input signal (AIN.VALUE ) offset or drift.
General Information
|
Type |
NV Parameter |
|
Units |
V |
|
Range |
–10 to +10 V |
|
Default Value |
0 V |
|
Data Type |
Float |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
Variants Supported
*In SynqNet
SynqNet is a digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices, a parameter may be available in the firmware but have no effect on the system. See .
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
/0 |
M_01-00-00-000 |
Related Topics
Block Diagram for Position/Velocity Loop (pg 1)