AOUT.VSCALE
Description
AOUT.VSCALE is an analog velocity scale factor that scales the analog output
(AOUT.VALUE) for AOUT.MODE = 1, 2, or 3. The value entered is the motor velocity per 10 V
of analog output. This value may be either higher or lower than the application velocity limit
(VL.LIMITP or VL.LIMITN), but the actual analog I/O will be limited by VL.LIMITP or VL.LIMITN.
General Information
|
Type |
NV Parameter |
|
Units |
Depends on UNIT.VROTARY or UNIT.ACCLINEAR Rotary: rpm/V, rps/V, (deg/s)/V, [(custom units)/s]/V, (rad/s)/V Linear: counts/s/V, (mm/s)/V, (μm/s)/V, [(custom units)/s]/V |
|
Range |
Rotary: 0.060 to 60,000 rpm/V Linear: 0.001 to 1.000 counts/s/V |
|
Default Value |
Rotary: 0.060 rpm/V Linear: 0.001 counts/s/V |
|
Data Type |
Float |
|
Start Version |
M_01-00-00-000 |
Variants Supported
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
/5 |
M_01-00-00-000 |
Related Topics