LOAD.INERTIA
Description
LOAD.INERTIA sets the load inertia.
General Information
|
Type |
NV Parameter |
|
Units |
kgcm² for rotary motors kg for linear motors |
|
Range |
1 to 1,000,000 kgcm² or kg |
|
Default Value |
0 kgcm² or kg |
|
Data Type |
Float |
|
See Also |
N/A |
|
Start Version |
M_01-03-06-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
/0 |
M_01-03-06-000 |
Related Topics