MOTOR.IMID
Description
The value of IL
"Instruction list"
This is a low-level language and resembles assembly.IMID can be estimated using the motor name plate information.
The following rule should generally be used:
In which Id is the value for IL.IMID, the preset rotor flux building current, Ir is the name plate phase current, cosϕ is the name plate power factor at rated and operation, and 0.8 is an empirical factor (accounts for the angle error due to voltage drop on the leakage induction).
General Information
|
Type |
R/W |
|
Units |
Arms |
|
Range |
0 to DRIVE.IPEAK |
|
Default Value |
0 |
|
Data Type |
Float |
|
Start Version |
M_01-08-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
/0 |
M_01-08-00-000 |
Related Topics