MOTOR.TBRAKEAPP
Description
This parameter is used to configure the mechanical delay required for the motor brake to close. The AKD will servo to hold position for the time set, allowing the brake to apply.
-
-
If MOTOR.AUTOSET = 1 and FB1.MEMVER > 0.01, this parameter will be automatically configured for Kollmorgen motors.
General Information
|
Type |
NV Parameter |
|
Units |
ms |
|
Range |
0 to 1,000 ms |
|
Default Value |
75 ms |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
/0 |
M_01-00-00-000 |
Related Topics