MOTOR.VOLTMIN
Description
This parameter configures the drive for the induction motor's minimum voltage at standstill. It is given as a percentage (%) of the motor’s rated voltage. MOTOR.VOLTMIN is used to calculate the constant volts per Hertz characteristics of the drive and motor and should be set to a value that generates a current of about 40% of the rated current at standstill.
General Information
|
Type |
NV Parameter |
|
Units |
% |
|
Range |
0 to 100% |
|
Default Value |
2% |
|
Data Type |
U16 |
|
See Also |
|
|
Start Version |
|
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
/3 |
M_01-00-00-000 |
Related Topics