VBUS.OVFTHRESH
Description
VBUS.OVFTHRESH reads the over voltage fault level for the DC bus.
This value is read from the drive EEPROM and varies according to the drive type.
General Information
|
Type |
R/O Parameter |
|
Units |
VDC |
|
Range |
0 to 900 VDC |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
See Also |
VBUS.UVFTHRESH |
|
Start Version |
M_01-00-00-000 |
Related Topics
1 Regeneration