VBUS.UVWTHRESH
Description
If VBUS.VALUE value drops below VBUS.UVWTHRESH, then a warning is generated.
General Information
|
Type |
NV Parameter |
|
Units |
VDC |
|
Range |
0 to 900 VDC |
|
Default Value |
10 volts above the default value of the under voltage fault threshold (VBUS.UVFTHRESH). The default value of VBUS.UVFTHRESH is hardware dependent. |
|
Data Type |
U16 |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
/0 |
M_01-00-00-000 |
Related Topics
1 Regeneration