FBD variables
"Function block diagram"
A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks diagrams using small boxes.
- Press the following button in the FBD toolbar to insert a variable tag:

Insert variable: In this mode, the mouse is used for inserting variable tags. Click in the diagram and drag the new variable to the desired position. - Double-click on a variable tag to open the variable selection box
- Either select the
symbol of the desired variable or enter a constant expression.
Variables tags must then be linked to other objects such as block inputs and outputs using connection lines.
- You can resize a variable box vertically in order to display, together with the variable name, its tag (short comment text), its description text, plus its I/O location if the variable is mapped to an I/O channel.
The variable name is always displayed at the bottom of the rectangle:
tag description %location name
For more details on Variable Tag and Description, see "Variables tab"