INSERTPLCopen motion icon

FunctionClosedA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Insert characters in a string.

Inputs

IN : STRING   Character string
STR : STRING  String containing characters to be inserted
POS : DINT    Position of the first inserted character (first character position is 1)

Outputs

Q : STRING   Modified string.

Remarks

The first valid character position is 1. In FFLD language, the operation is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung.

In ILClosed"Instruction list" This is a low-level language and resembles assembly, the first input (the string) must be loaded in the current result before calling the function. Other arguments are operands of the function, separated by comas.

ST Language

Q := INSERT (IN, STR, POS);

FBD Language

InsertFbd.gif (1386 octets)

FFLD Language

(* The function is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)
InsertLd.gif (1642 octets)

IL Language:

Op1: LDClosed"Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them     IN
     INSERT STR, POS
     ST     Q

See also

+   MLEN   DELETE   FIND   REPLACE    LEFT   RIGHT   MID