MLPrfReadOScale
Description
Returns the Output Ratio value of a selected CAM Profile. Ratios can be changed on the fly to modify the CAM Profile while maintaining its basic shape. A change in output ratio is equivalent to stretching, and flipping if negative, the CAM Profile on the Y (or Output) Axis.
Arguments
Input
ProfileID |
Description |
ID number of an initialized CAM Profile |
Data type |
DINT |
|
Range |
[-2147483648, 2147483648] |
|
Unit |
N/A |
|
Default |
— |
Output
Ratio |
Description |
Returns the Output Ratio of the selected CAM Profile |
Data type |
LREAL |
|
Unit |
N/A |
Related Functions
Previous Function Name
Example
Structured Text
//Save value of output ratio CamRatio := MLPrfReadOScale( Profiles.Profile_A );
|
Ladder Diagram
Function Block Diagram