ACTION#.CONDITION

Description

This keyword defines the condition to test the action source for. If the value is 0 (always), then no test is performed and the condition always passes.

The available values of this parameter depend on the value of ACTION#.SOURCE. If the source is changed, the available range may be updated and the condition will be reset to default. Available conditions are:

Value Description
0 Always passes
1 Is false
2 Is true
3 Less than
4 Greater than
5 Rising EdgeClosedA rising edge is the transition of a digital signal from low to high. It is also called positive edge
6 Falling Edge
7 Rises above threshold
8 Falls below threshold
9 Rising Edge (triggers on high at start)
10 Falling Edge (triggers on low at start)
11 Is Equal To
12 Becomes Equal To

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

Depends on ACTION#.SOURCE

Default Value

0 (always)

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.