ACTION#.SOURCEID
Description
Some action sources require a specific source ID number. For example, if your action source is a Digital Input, then a source ID of 1 would correspond to Digital Input 1.
The range of the source ID will depend on the value of the corresponding source. If the source is modified, the range and units of the source ID may change, and the source ID value will default to the first valid value.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Depends on ACTION#.SOURCE |
Range |
Depends on ACTION#.SOURCE |
Default Value |
0 |
Data Type |
Integer |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported