ACTION#.TASKPARAM
Description
Some tasks require a Task Param value to specify what is acted upon. ACTION#.TASK must be set before ACTION#.TASKPARAM. If ACTION#.TASK is modified, then the range and units of ACTION#.TASKPARAM may be modified, and the value will be defaulted.
Not all tasks require a task param.
Example
This example shows an action which starts a motion task 4 on AXIS1
>> ACTION1.TASK = 5 (Launch motion task)
>> ACTION1.TASKID = 1 (AXIS1)
>> ACTION1.TASKPARAM = 4
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
Depends on ACTION#.TASK |
Default Value |
Depends on ACTION#.TASK |
Data Type |
Float |
Stored in Non Volatile Memory |
Yes |
Task Parameter values for certain tasks
Task: Set the Command Source and Op-Mode for an axis.
Command Source and Op-mode combination | Value |
---|---|
Service/TorqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist | 0 |
Service/Velocity | 1 |
Service/Position | 2 |
Service/No Change | 9 |
FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design/Torque | 10 |
Fieldbus/Velocity | 11 |
Fieldbus/Position | 12 |
Fieldbus/No Change | 19 |
Electronic Gearing/Position | 22 |
Analog/Torque | 30 |
Analog/Velocity | 31 |
Analog/Position | 32 |
Analog/No Change | 39 |
No Change/Torque | 90 |
No Change/Velocity | 91 |
No Change/Position | 92 |
Variants Supported
All variants are supported.