AXISx.OBS.BW

Description

AXIS#.OBS.BW sets the frequency at which the observer starts being the dominant component in the velocity signal.

Versions

Action Version Notes
Implemented 02-04-03-000  

General Information

Type

Read/Write

Units

Hz

Range

1 to 8,000.000

Default Value

500

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.