AXIS#.PL.OFFSET

Description

This parameter sets an offset that is applied to AXIS#.PL.FB.

Examples

The position feedback is at 1000 [deg]. AXIS#.PL.OFFSET is set to 500. The new position feedback is 1500 [deg].

-->AXIS1.PL.FB

1000.000 [deg]

-->AXIS1.PL.OFFSET 500

-->AXIS1.PL.FB

1500.000 [deg]

Versions

Action Version Notes
Implemented 02-01-04-000  

General Information

Type Read/Write
Units

Rotary: counts, rad, deg, custom units, 16-bit counts

Linear: counts, mm, µm, custom units, 16-bit counts

See Position Units for details.

Range Depends on units. See Position Range for details.
Default Value

0 counts

Note: Default is adjusted to account for the units selected by the user.

Data Type Float
See Also  

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.