AXIS#.WS.NUMLOOPS

Description

This parameter sets the maximum number of wake and shake repetitions. AXIS#.MOTOR.PHASE is calculated as mean value of all wake and shake repetitions.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

counts

Range

0 to 20 counts

Default Value

5 counts

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosedPDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.WS.NUMLOOPS 0x5013 0x2 USINT - - RW False
AXIS2.WS.NUMLOOPS 0x5113 0x2 USINT - - RW False