AXIS#.IPEAK

Description

AXIS#.IPEAK returns the drive peak rated current in Arms.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Arms

Range

N/A

Default Value

N/A

Data Type

Float

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosedPDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.IPEAK 0x5000 0xC DINT 1000:1 - RO False
AXIS2.IPEAK 0x5100 0xC DINT 1000:1 - RO False